AXIS#.CANOPEN.GEARPRIMARY.SHAFTREV
Description
This keyword provides the count of driving shaft revolutions for the primary position gear ratio calculation. It is part of the scaling calculation used for CANOpenCANopen is a communication protocol and device profile specification for embedded systems used in automation for fieldbuses working in real time objects.
Context
See Scaling.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type |
Read/Write |
Units |
N/A |
Range |
1 to 4294967295 |
Default Value |
1 |
Data Type |
Integer |
Stored in Non Volatile Memory |
Yes |
Variants Supported
CANBus and EtherCat
Fieldbus Information
CANopen |
|
Index |
6091h |
Subindex |
2 |
Data Type |
U32 |
Float Scale |
1:1 |
Access |
Read/Write |
PDO Map | No |